Other Parts Discussed in Thread: EV2400, , BQSTUDIO
Hello,
I am using the BQ34Z100EVM connected to a 12V 12Ah lead acid battery and the EV2400 interface . I followed the instructions in the datasheet, calibrated the board several times. But even when there is no load connected it measures between 8-10mA consumption.
I created a log file needed to get a suitable chemID (charge-relax-discharge-relax).
But, because of that current the Gauging Parameter Calculator returns the chemID of a 7200Ah battery and a warning that the current is not 0 in the relaxation period.
Thank you in advance!
Best regards,
Mozes Arpad