This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TLV61046A: TLV61046A

Part Number: TLV61046A
Other Parts Discussed in Thread: TLV61046

Tool/software: WEBENCH® Design Tools

Hi, please help me about power IC TLV61046. I use TLV61046 with Vin = 2~3.5 V ( DC), Vout = 12.5V ( DC), when i add resistor load with load current about 50ma, It is running good. When i add OLED load ,Load current range from 30~ 40ma, whistles from the inductor comming out, why dose is it and what is the solution? Please help me, Thanks !

PM : To Minqiu ,I press the wrong "resolved" button, but i am still wait your reponse