Hi,
We've done testing our own board. The SPI is working fine. But we still cannot measure 1MHz square waveform between CEXT1 and CEXT2.
SPI can return what command I just send. Fault code is 0b000. We only connect SDI, SDO, CLK, CS, RESET to our MCU.
DIR, DIR_RT, EN, DONE are all floating.
Issue:
Does the internal 1MHz clock work after power-on? 12V and 5V is all set. Or I need to setup any GPIO for finish EMB1428 internal clock initialization?
BR,
Troy