Other Parts Discussed in Thread: GPCRB
I am using this IC in a drone application where the ambient temperatures can range from -20C to 50C. The cell temperature ranges from ~0C up to 65C depending on the environmental conditions, though, they are usually biased around the outside temp (colder days yield colder batteries, hotter days yield hotter batteries).
I have noticed some estimation inaccuracies when my battery is in the extreme heat and I am wondering if my settings for these two parameters: T rise, and T time constant, are correct. Can you provide an explanation of these two parameters and mention how they effect the IT algorithm? Information I have seen in data sheets do not provide any information on these parameters.
Thank you,
> Andrew