This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/UCC39002: UCC39002

Part Number: UCC39002

Tool/software: WEBENCH® Design Tools

Dear TI friend:

I use UCC39002 demo HPA027A designed chare electric current circuit; two power module output voltage Vout=12V,Iout(max)=50A, use Vout+ as sampling and the sampling resistor is 1mΩ, CSO amplification times set is 100, Power supply voltage adjustment range ΔV=0.6V;
 1.full load, There will be times (tens to hundreds of milliseconds) when the current is very uneven, then circuit can share; waveform as attached;

2.Underloading (below 7A, load mode are CC or CR) the output current of the two power sources keeps oscillating, as attached;

so can you help check the questions?

Thank you!