Hello,
I am having an issue with my 7 cell balancing design using the BQ77915. I am using resistors and a power supply to test my PCB. Below are the voltages I am seeing for each module (each voltage is referenced to the local VSS of each device):
TOP:
- PRES = 15.47V
- VDD = 15.48V
- AVDD = 3.05V
- CCFG = 3.05
- DSG = 12.58V
- CHG = 12.58V
- TS = 0V (This did not make sense to me)
- LD = -11.64V
- LPWR = 3.05V
- CBI = 2.26V
BOTTOM:
- PRES = 14.66V
- VDD = 11.62V
- AVDD = 3.03V
- CCFG = 0V
- DSG = 0V
- CHG = 0V
- TS = 0V
- LD = 0V
- LPWR = not connected
- CTRD = 12.04V
- CTRC = 12.04V
Attached is my schematic for reference. Please note: the pres pin for the top device in the stack is pulled up to PACK+ through a 10K resistor. Also, I modified the TS pin connections for each device in the stack. Instead of using an NTC for each, i used a 10K resistor to simulate ambient temperature.
Please let me know if you need any additional informationBQ77915.pdf