Other Parts Discussed in Thread: TPS61022
Tool/software: WEBENCH® Design Tools
Hello Sir,
I use the TPS611781 for a 5V output without load disconnect function design, and the EN pin is PD/100K to GND to disable.
But use the 4.2V for Vin and got a 3.7V in the Vout when the EN pin is low, if add PU/3.3V on the EN pin and got the output is correct 5V.
Could you give me a advice for the PD EN pin and got the 3.7V in the Vout?
Sincerely,
John