Part Number: TPS544C20
Hi Experts,
I want to know hiccup phenomenon. Would you answer a following question?
1. If I set hiccup mode and TPS544x20 detects OC_FAULT(STATUS_WORD low byte bit 4 is set "1"), PGOOD will goes low. Is my understanding correct?
2. If so, STATUS_WORD high byte bit 3 is also set "1", correct?
3. If so, is it possible to STATUS_WORD high byte bit 3 is not set "1"?
4. If TPS544x20 detects OC_Fault, TPS544x20 will work by hiccup mode, correct?
5. If OC_Fault condition removes very quickly after OC_Fault detected, does TPS544x20 skip the hiccup mode?
Your support would be much appreciated.
Best Regards,
Fujiwara