Other Parts Discussed in Thread: BQ78350, , BQ76200, BQ2970
Hello,
I've got a question regarding hardware overcurrent protection in BQ796022 (working with BQ78350). There is a programmable threshold limit on current sense input (form 22mV to 200mV), so depending on shunt resistor value it turns off battery when the current exceeds the limit.
Is there any possibility to bypass this protection (apart of lovering the value of shunt resistor) so that device limits the current instead of causing battery to disconnect?
Because working with BLDC motor high currents spikes can occur.
Thank you for any support,
Adam