Hi,
Recently,I used BQ25606 in my project,the part of schematics are as follows:
In fact, The VBUS using a adapter :12V/1A。The battery is 2600mAh.
usually,sys load current about 300-500mA,LED Foward Voltage is about 2V,The charging current is close enough to the setting value,I've measure PMID about 11.9V,REGN is 6V,TS is 3V,but,when I charged a battey which initial voltage is about 3.5V,the stat LED and PG status is correct,after charged 8 hour or more,the STAT LED Blinking at 1Hz, at this time,the VBAT Voltage is close enough to 4.2V,PMID still about 11.9V,REGN is 6V,TS is 3V,if I remove the same battery and plug in again quickly ,after a while,the stat LED back to normal , stat indicator is HIGH,I‘m confused !! why?? Why does timer fault happen ?Even if I increase the charging current to 1A,this situation still exists. By the way,the D+ D- do not connect anaything. Why does timer fault happen ?
Best Regards