This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25982: SOA and max Cout

Part Number: TPS25982
Other Parts Discussed in Thread: LM5069

What is the max value of Cout for TPS259827, operated at Vin=24V? I saw this question already in the forum, but the discussion went to private. 

Could you please provide a diagram with the SOA of the internal FET? 

For industrial 24V rails an OVLO >=26V would be an very interesting feature! Do we've such a device on our roadmap? 

  • Hi Reimer,

    If the load is only purely capacitive during startup, there is no limit on the amount of Cout. You can increase dv/dt capacitor value to reduce Vout slew-rate (and hence inrush currents) to support large Cout.

    What is the target Cout ?

    We won’t provide SOA data for any of our integrated devices because we always ensure device protection through inbuilt over temperature protection.

    For roadmap, please email me.

    BR, Rakesh

  • Hello Rakesh

    We (industrial customer of Hanno) are currently developing a new universal power supply.

    With regard to the IEC 62368-1, this power supply should have 6 separate output voltages, which have a eFuse / Hot plugging characteristic

    • Our current systems (controllers with external FET) are for switching on a capacity of max. 4700μF specified.
    • In addition, when switching on we assume a load current of 24V / 24Ohm = 1A.
    • Switching on thus has an ohmic (=> 1A) and capacitive (=> 4.700µF) component.

    For the TPS259827LNRGE we have considered a current limit of 6A, with short-term currents (ca. 50ms)  up to 9A should be possible.

    So far, we use the PSMN7R6-100BSE.
    Without an overview of the SOA, we can not currently assess the limits of the IC

    Can the TPS259827LNRGE turn on a 4.700μF / 1A load? Where are the limits?

    Best Regards

    Ralf

    koerfer.ralf@scheidt-bachmann.de

  • Hi Ralf,

    Welcome to E2E and thanks for sharing the information

    We have design calculator to check the load boundaries during startup. It is available at http://www.ti.com/product/TPS25982/technicaldocuments

    Please use that and let me know if you have any questions.

    BR, Rakesh

  • Hello Rakesh,

    Using the Excel tool and Figure 53 (data sheet page 34), the max. Output capacity can be determined.

    • At VIN = 24V and a load current of approx. 0.5A   => max. Output capacitance of approx. 265μF (@CdV / dt = 10nF).
    • At VIN = 12V and a load current of approx. 0.5A,  => max. Output capacitance of about 1,800μF (@CdV / dt = 22nF).

    For our application, these values are too small, we continue to take the LM5069.

    Best regards

    Ralf

  • Hi Ralf,

    Understood.

    One way is to use PG signal to enable the downstream load so that during startup the load will be purely capacitive which can be handled with appropriate CdV / dt.

    BR, Rakesh

  • Hello Rakesh,


    Thank you for your feedback signal.
    • With TPS259827, at IOUT = 0A only max. 600μF switch-on capacity possible.
    • In our applications we need a higher performance.

    This efuse is a very interesting IC especially with regard to the IEC 62368-1 certification.
    It would be nice if Texas Instruments could include a more powerful version in their product program in the future:
    Ideally  with integrated FET and enhanced SOA:
    • VIN = 28V Recommended, absolute max. 35V
    • IOUT = 15A
    • COUT = max. 2,000μF with additional ILOAD  = 0,5A

    Can you please close the ticket.

    Best regards
    Ralf