This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: Inrush and CSS

Part Number: TPS2121


Dear Arthur,

one question if we want that inrush be 500mA and the CL is 280uF (Vin = 5V9

We get the calculation SR_ON = 1785V/s.

in your Table 1 in DS you only have for 780V/s = 100nF

How can i calculate the CSS for SR=1785V/s ? 

Also there is figure 6 on page 9 in DS but there are different values as in table 1 ?

in table 1 100nF = 780V/s and in figure 6 100nF = 3.5V/ms = 3500V/s

Best Regards,

D. 

  • Hi D,

    Unfortunately, I can only provide some back of the envelop calculations for this question.

    I cannot provide a direct equation for the Css capacitor but it is possible to use linear interpolation between the points.

    When Css capacitance is dropped by a factor of 10, Slew Rate increases by a factor of 10 (approximately).

    Hence linearly interpolating between 100nF and 10nF (with corresponding slew rates of 780V/s and 7800V/sec), I would say that you need a Css capacitance around 85nF to get a Slew Rate of 1800V/s.

    Do note that this is only an approximate calculation.