Dear Sir/Ms.
I read the specification of TPS92692, I have some questions about the content. Can you consult with you?
1. We have an example of TPS92692EVM. In the Boost architecture, if Vin > Vout, will PDRV open -MOSET?
2. We have an example of EVM, can P-MOSFET be removed? If you don't need P-MOSFET, how to design? Is R2 shorted directly? How is Pin12 PDRV connected? Is it connected or connected to the ground?
3. The third and fourth questions are the same. Can the Resistor of CSN and CSP be placed on the Low Side? I have customers who want to use Low Side Sense.
4. We have an example of EVM, what is the Voltage Margin of CSN and CSP? The customer has this problem because of the extension of Buck-Boost? They want to know the design boundary of the LED? Is it filtered by the output capacitor? So the border can catch a little less.
The customer will ask the third and fourth questions because they want to make the output voltage higher, and the LEDs can be several strings.
5. The fifth problem is that the customer wants Class 5, which requires -18dB in this band of 76Mhz~108Mhz. According to their past experience, because of the spread spectrum, in the high frequency band, the signal strength after 76Mhz is more dispersed, and the filter is not well designed. So customers want to ask if there is any experience in TI that can be shared with them.
My English is not good. If you have any interesting sentences, please tell me. I will use another sentence to explain.
Best Regards,
Kami Huang