This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem with CEDV

Hello guys,

the project is to obtain the optimal parameters for our battery profile with the CEDV method.

The requirements are:

- 7 amps (lowrate) @ 2.5°C, roomtemperature and 45°C

- 15 amps(highrate) @ 2.5°C, roomtemperature and 45°C

Battery Specs: 

- 4 cells in series 

-14 cells parallel

- 58 volts end of charge 

- 39 volts end of discharge

Now the Problem: If i test the batterypack with 15 amps the BMS switches the battery off, because the cells exceed 60 °C cell temperature, so we do not have a chance to discharge the battery from 100% to 0% SOC. Is it a requirement to make a constant discharge with 15 amps at every temperature or can we vary the current for different temperatures. 

Thank you!