Other Parts Discussed in Thread: BQ25886, BQ25887
Hi Team,
My customer is using BQ24133 for a 2-cell battery charging solution.
The requirement for the 2-cell battery is 8.4V, 1A.
Considering the input is 10V, if targeting the efficiency 80%, the input current should be 0.96A. Is this achievable?
There's some concern about the voltage difference from 10V to 8.4V, only 1.6V. We want to check if it is possible to charge this 8.4V/1A 2-cell battery.
A second question is that, as this is 2 cell battery, is it necessary to use any charging balance scheme between the 2 cells?