Other Parts Discussed in Thread: AM5728,
Hi,
my question is related to the issue mentioned in https://e2e.ti.com/support/power-management/f/196/p/738631/2727879
We see the exact same situation as that the PMIC is resetting the AM5728 CPU although this is not only happening at -40 degrees but some boards have this issue already at room temperature.
In that case the board is resetting about 10 times(with intervals of maybe 2 seconds) and when the system is warmed up a little it doesn't happen anymore and works properly.
Not all boards have this issue but most do.
It is our own board using SDK 05.00.00.15 as basis
When the board starts u-boot it starts normally and when I interrupt the startup sequence of u-boot the board is working fine. But when Linux is starting the CPU is reset. I guess this is due to the fact that the power consumption is increasing. We see the same behavior on the scope screens as shown in the related issue.
At the moment my first question is if there was a solution found to the above mentioned article. It stopped without a solution and also I couldn't find any other message with the same issue.
Regards, Robert