This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R3-DEVICE-FW: "Discharge rate is too high" error during 24h-test

Part Number: BQ40Z50-R3-DEVICE-FW

Hi,
I've submitted a file according to http://www.tij.co.jp/jp/lit/an/slva725a/slva725a.pdf, (file attached)

As result, in GPC_report.txt I get:

"       0    0    0
Warning: Discharge rate is too high. High rate reduces ID detection accuracy     10 hr rate is recomeended. Total discharge time is less than 5 hrs     t_hrs=  1.08722222222222"

How can I fix this?

6180.roomtemp_rel_dis_rel.csv

ProcessingType= 2
NumCellSeries= 2
ElapsedTimeColumn=0
VoltageColumn= 2
CurrentColumn= 3
TemperatureColumn= 1