Hi, I realized that the buck charging circuit of BQ24765 allows current being supplied from the battery being charged. It happens due to the boddy diodes on the integrated fets. When the input source is removed, the circuit is being powered by the charged battery.