This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir/ Madam,
Please provide us the derating information (derating curve) for the parts,
TLV62095RGTR
SN74LVC2G34DCKR
SN74LVC1G18DBVR
TPS74401RGWT
Thanks & Regards,
Vyshnav Krishnan
Hi Vyshnav,
typically, the maximum operating junction temperature for these devices as well as their thermal resistances are given in the corresponding datasheets.
The derating can be calculated for each device using these parameters together with the application specific power dissipation.
Hi Vyshnav,
it can be calculated using ohms law - but with temperatures and thermal resistances instead of voltages and ohmic resistances.
An example:
Datasheet Values:
- Thermal resistance Junction to Case: 50°C/W
- Maximum operating Junction temperature: 125°C
Design specific values:
- Case Temperature: 70°C
Resulting maximum permissible power dissipation:
(125°C - 70°C) / 50°C/W = 1.1W abs. max.
Dear Bjoern Goerner,
Thank you. I will follow the same steps to find derating characteristics for the other IC's as well.
Best Regards,
Vyshnav Krishnan