Hi,
Did tests with TLV70233DSE in a design where there for historical reasons is 10k in series with the EN pin (between MCU control pin and LDO EN pin) and noted that when driving the MCU pin low the EN pin did not go to 0V, but rather to 200mV. My input voltage is ~4.5V, so I was considering that perhaps there is an internal pull-up of ~200kOhm that explains this behavior, forming a voltage divider with my 10k. However, I do not find any such indication in the datasheet.
Is there any internal pull-up (or pull-down) on the EN pin?
Thanks!