This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC20225: SOIC package availability

Part Number: UCC20225
Other Parts Discussed in Thread: UCC20520

Dear sir,

Could you suggest any driver IC similar to UCC20225 (operating temperature : -40degC to +125degC, which is having complimentary low side drive with dead-time adjustment and which is also having SOIC type package availability. UCC20225 is only available in LGA package.

Thanks,

Nesh

  • Hi Nesh,


    Thank you for your question. I work on the applications team in the high power drivers group.


    UCC20520 is a dual channel isolated gate driver with single input. It comes in a 16 pin SOIC package with recommended operating temperature range of -40 to 125 °C. UCC20520 is equipped with a similarly functioning dead time circuit as UCC20225 where the value of a resistor tied between the DT pin and GND adjusts the dead time duration.


    If you have any more requirements, feel free to ask and I can revise my recommendation.


    If this answered your question, could you please press the green button? If not, feel free to ask more questions.


    Thanks and best regards,
    Zach

  • thanks a lot sir for the reply