This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team
As you can see in the picture, I used 10K as the value of Rpu in my design. But in the datasheet of TPS3702, the range of IUV is 0.3mA to 10mA. so I want to ask;
1. If I used 10K as the value of Rpu in my design, the IUV is 0.33 which is closed to the IUV(min), is there any risk when IUV closed to the IUV(min)? please kindly explain it specifically.
2. Why you put the IUV IOV current limit in the datasheet, it seems that this spec won't cause any issue when use the TPS3702, could you help me understand that?
Thanks
Best reagrds
Wesley huang
Hi Wesley,
For your question, this should not be a problem. If you look at our absolute maximum ratings, we actually specify ±40 mA as the range for IUV and IOV. Although we recommend 0.3 to 10 mA, getting close should not be a big issue. We put the current limits on the datasheet because operating at the edges could cause issues maintaining a stable output voltage. I don't think low output current should be an issue, however.
Thanks,
Abhinav.
Hi Abhinav
Thanks for your answer. I still have two questions.
1. Could you explain more specifically about why operating at the edges could cause issues maintaining a stable output voltage from the perspective of low IUV
2. Could you specifically explain the consequence when output voltage is unstable?
3. Could you please recommend a Rpu based on the design I have put in the former reply?
Thanks
Best reagrds
Wesley huang
Hi Wesley,
I can reach out to the design team for a little more clarity on the issues with using certain pull-up resistances. That being said, you should use a 10k resistor for Rpu, as is also used in the EVM.
Thanks,
Abhinav.
Hi Abhinav
Thanks for your answer and Rpu recommendation .I hope that I could get the answer as soon as possible.
Thanks
Best regards
Wesley huang
Hi Abhinav
Thanks for your answer. I still have a questions.
1. the 8.2.2.2 just mentioned about the pull-up voltage does not exceed the sink-current capability of the device, but it still can't explain why the Rpu can't not be selected the too large value.
Thanks
Best reagrds
Wesley huang
Hi Wesley,
The resistor cannot be too large to affect the recognition of logic low levels on the output. A in-depth and careful analysis of this is provided in Choosing an Appropriate Pull-up/Pull-down Resistor for Open Drain Outputs. This app note will help analyze the range that is appropriate.
Thanks,
Abhinav.