This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54519: Schematic Review Request for EVM

Part Number: TPS54519


Hi Team,

I am designing a reference EVM for a high-speed retimer board and would like to use the TPS54519 because of its efficiency in sourcing up to 5A. I have two versions of the board that will both take VIN = 3.3V, but one version will require that the regulator output 2.5V, while the other version requires a regulator output of 1.2V. I have implemented a 3-pin shunt header that will have a noticeable silkscreen message to inform the user how to set the shunt headers.

Can you help review the schematic and let me know if anything is missing? I used the TPS54519EVM as a reference. 

One additional question I have is whether there are any smaller size inductors that you would also recommend aside from the Coilcraft one?

Thanks for your help!

DS560AR8XX_1P2V_DCDCs_Sch.PDF

Michael