This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: Recommend chip

Part Number: UCC28950

Hi,

I want to design a charger. The output power is about 800W and the efficiency is more than 90%. The input voltage is AC 180~265V, the output voltage is DC 70~85V and the output current is 10A.

Could you please recommend a suitable chip for me? And the suitable structure or reference design?

Thanks.

Kevin Xiong