Hi team,
My customer has been using LM3526MX-L/NOPB and provided some questions as follows.
- They has been using this device over 10 years but it failed at output short test for a few months.
Is there any design/process change for this device recently? -
At CURRENT LIMIT section, it describes that “~ limits the output current to approximately 1.0A typical”.
On the other hand, SOFT START section describes that “the maximum in-rush current is internally limited to 1.5A”
Is those difference just from Typ and Max value of Isc? - Although datasheet describes that “the maximum in-rush current is internally limited to 1.5A”, figure.15 shows that about 2Apk inrush current before current is limited to 1A.
A similar phenomenon(4Apk inrush current was observed before current limit) was observed on the customer's board.
Is this correct behavior for this device? - What is difference between ISC(Short Circuit Output Current) and OCTHRESH(Over-current Threshold)?
I'm looking forward to hearing back from you.
Best regards,
Shota Mago