Other Parts Discussed in Thread: UC1844A
Hello Everyone,
Currently, we are working on a flyback converter of 120W output. We are using UC3843A in which we are getting output but we are facing many problems which are listed below:-
1. The below circuit diagram is used for the startup of the IC , the IC gets to start at 8.8V but gets immediately gets turn off after giving a small pulse off output whereas we have referred the same application in datasheet of UC3843A, moreover as per the datasheet the IC should get turned off at 7.6V but we are getting turned off at 8.4V (the analysis for the same is attached in the below video).
2. Can you please help us the better/best way to power up the iC apart of the tertiary winding as we don't want to go with it.
Thanks in Advance
Regards