Other Parts Discussed in Thread: BQSTUDIO, BQ34Z100
Dear sir,
I'm using BQ34z100-G1 for gauging.
My battery pack specs are :
13s13p NMC cells.(LGC 18650-M26 2600mAh/2500mAh)
Nominal voltage 46.8V
Charging volatge 54.6V
Charging current 10A
Max discharge current 45A
Capacity 33.8Ah
Shunt resistor value 1m-ohm.
Can you please help me setting the data flash parameters using bqstudio?
Scaling factor is 2X.
What should be the Taper current, Quit current, Qmax cell0, current at EOC etc?
Regards,
Samruddhi