Hi, the data sheet of the TPS63060 shows a chip with 2+2 power GND but the the spec of the
DSC shows 4+4 power GND. Which one is the correct one?
You mentioned that the irush could be limited by raising the FB. How? I have only need for max 500mA
current and a slow start is perfectly ok since it will not load the battery and cables as much and
make the system more stable.