(1) Power-on-reset(POR) is described in the page 19 (Device Operation) of TPS2544 datasheet.
(1-1) Does POR mean that VIN is 0V and EN is low?
(1-2) And after VIN is 5V and EN is high, CTL configuration is detected?
(2) Is it correct that the following (a) and (b) are the same state?
(a) EN is low.
(b) CTL setting is DCH(Discharge) (CTL1, CTL2, CTL3) = (0, 0, 0).
(3) When DCH(Discharge) (000X) is set, VBUS off (discharge) happen for two seconds every time. Is it correct?
Thank you.
Katsuhiro