Hello Expert on Power management
can any one explain the the calculation of power rating the R sense ?
i use the BQ24703EVM for reference : http://www.ti.com/lit/ug/sluu160a/sluu160a.pdf
i want to make the current charging is 10 A, so i should change the R20 become 0.005 Ohm on that schematic to make sure the SRSET input not more than 2.5 V (the max can be)
will very helpful if any body have done the BOM to make the 10A current charging
Many thanks