Is the behavior of the \FLT output defined when the LM76202 V(in) is below V(porr)?
I am developing a design using two LM76202-Q1s in a diode-OR configuration, and am trying to determine if I can monitor the state of each LM76202 sufficiently with just the \FLT pin, or if I must also monitor the input voltage to each LM76202 and consider it disabled if V(in) < V(porr) OR \FLT asserted.