This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This spec falls under the isolated flybuck converters line but I don't see any information regarding the isolation specs on the datasheet. Is it rated for 1.5kVrms or 3kVrms isolation?
Hey again Lauren ,
The isolation transformer on the LM5019 EVM is the same series, Coilcraft LPD5030V-154ME so it also has a 1.5kV isolation rating. You can also use a higher isolation transformer from the magnetics vendor.
Are you specifically looking for 3kV isolation?
-Orlando
Hi Orlando,
Yes, I need up to 3kVrms. This is for an auxiliary power supply in a grid infrastructure application (helping a customer find a part recommendation).
Would you happen to have any other suggestions? Requirements are (including 3kVrms isolation) 2 W output, 12V-20 V input, 20V output, working voltage needs to be 50-60V, sometimes 600V (in a worst case scenario), and really needs to be pretty simple to design in. They have a preference for flybuck topology.
If not then no worries I can keep looking. Really appreciate the help!
Thanks,
Lauren
Hi Lauren,
I found a decent isolation transformer, the Wurth 750343953 with 3.75kVAC isolation from TIDA-010006.
https://www.we-online.de/katalog/datasheet/750343953.pdf
I'm not sure what the working voltage is and the extra windings are unnecessary, but otherwise it will work in a Flybuck topology.
I will look into my magnetics contacts and see if they have a better transformer and let you know,
-Orlando