Hi Jeff,
As we have discussed here
https://e2e.ti.com/support/power-management/f/196/t/845657
Improper values of switching inductor and output capacitors will cause large input current of about 30mA when there is no battery being charged.
As the datasheet says, To get good loop stability, the resonant frequency of the output inductor and output capacitor should be designed between 15 kHz and 25 kHz. With 2.2-µH inductor, the typical output capacitor value is 20 µF.
Now in my design, I use 1uH+44uF, but sometimes the current is about 30mA, could you help to investigate further to explain such situation?
Thanks.