Other Parts Discussed in Thread: TPS7A91, TPS51200, TPS82140, TPS7A89, TPS82130
Hi TI team,
I'm using the following regulators of TPS family in our upcoming board.
TPS family:
TPS7A85: 1.2V@4A
TPS7A85: 1V@4A
TPS7A91: 1.8V@50mA
TPS51200: 0.75V VTT Termination and Vref
TPS82140: 1.5V@2A
TPS82140: 2.8V@2A
TPS7A89: 3.3V@2A
TPS7A89: 2.5V@2A
TPS82130: 3.3V@3A
Kindly verify the attached schematics for the above circuits.
Thanks and Regards,
Binayak