Other Parts Discussed in Thread: PTD08A020W, PTD08D210W, PTD08A010W
I copy KC705 power solution in my design. I download the .XML file from Xilinx website,and use TI-Digital-Power-Manufacturing-Tool to configure UCD9248. But the log told me many error happened. Such as "READ_VOUT on rail #2 (0.300 V) was not within 3% of VOUT_COMMAND (1.800 V)". And just five of the power rail turn on, the other six power rail can turn on. I try to measure the signals and analyse the reason, I found UCD9248 didn't send the signals to the power modules . Please help me to anlyse this ploblem.
Please refer the schematic as attachment.4431.Power.pdf
I list some infomation in the table below:
| controller | power module | Power name | voltage | other |
| UCD9248PFC | PTD08A020W | VCCINT_FPGA | 1V | PWM OK |
| PTD08D210W | VCCAUX | 0V | PWM keep low | |
| VCC3V3 | 0V | PWM keep low | ||
| PTD08A010W | VADJ_FPGA | 2.65V | PWM keep low | |
| UCD9248PFC | PTD08D210W | VCC2V5_FPGA | 0.3V | PWM keep low |
| VCC1V5_FPGA | 0.75V | PWM keep low | ||
| PTD08D210W | MGTAVCC | 1.0V | PWM OK | |
| MGTAVTT | 1.23V | PWM OK | ||
| UCD9248PFC | PTD08D210W | VCCAUX_IO | 0V | PWM keep low |
| VCCBRAM | 1V | PWM OK | ||
| PTD08A010W | MGTVCCAUX | 1.83V | PWM OK |