A follow-on question for locked "LM5060: Idea Check"
As the voltage of each battery may vary, it is possible the battery with the highest voltage supplies power to the whole system. If this battery is disconnected, will this LM5060 + LM74700 solution provides the seamless switchover to other batteries without interrupting output power (e.g. significant voltage drop), will it require a supercap at the output as the max current is 150A?