Part Number: BQ40Z50-R3-DEVICE-FW
Hello,
I read on the forum the steps to create the golden file should be :
1. Run the Optimization Cycle to update Qmax and the Ra-table
2. Go to the Data Flash window and press the Read All button
3. Export the gg.csv file
4. Edit the gg.csv file using a text editor. e.g. Notepad. Do not use Excel.
5. Set the Update Status to 02 and set the Cycle Count to 0.
6. Load the default .srec file into the device.
7. Load the ChemID into the device.
8. Load your modified gg.csv file into the device and press the Write All button
9. Save the golden .srec file.
Is is possible at the end of the leaning cycle to modify manually in Bq studio the update status to 02 and cycle count to 0, then to click on Write_All and just go to the tab firmware and then Read Srec to save the golden file. That would save the need to use a text editor? It seems to work but maybe I missed something.
Best regards,
Clement