This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596: Output capacitor and Inductance determination.

Part Number: LM2596

If the maximum output current is less than 0.6 Amps, do I have to assume 0.6 Amp is the maximum output current as there is no a lookup graph to find the inductor value.

  • Hello,

    I would recommend visiting section 9.1.5 and 9.1.6 starting from page 17 of the datasheet. There is a comprehensive look-up table given on page 19 for appropriate inductor selection. 

    Best Regards,

    Ankit Gupta

    Application Engineer.

      

  • If you see on page 19 of the data sheet the minimum  maximum load current shown is 0.6 Amps. In my design my maximum load current is 0.25 Amps so, I am not sure what max. load current to use in order to select the inductor value.

  • Hello Afework,

    Looks like your application is of the discontinuous mode of operation, which is helpful for light-load efficiency. I would recommend you using an inductor smaller than 15uH. I normally recommend inductors to have saturation current higher than part's current limit, because your inductor should not saturate during the current-limit protection scenario. So I would recommend having an inductor less than 15uH and Isat greater than 6.9A. And I would recommend double-checking the stability of your design on the Webench. Hope this helps!

    Please close the thread if you think my response answered your question.

    Best Regards,

    Ankit Gupta

    Application Engineer