Other Parts Discussed in Thread: ADS8528, TLV62565, LMR10515
Hello,
We have been having FPGA I/Os go bad and we think it might be caused by the 3.3V LM2831 regulator supplying power to it. The maximum FPGA's maximum allowed I/O power supply voltage is 3.6V.
After power is initially applied, the output of an LM2831 goes up to 3.860V (as shown in the image below, Nominal voltage is 3.3V). The input is fed by the 5V output of another LM2831.
What can we do to reduce the voltage overshoot?
Thanks,
Stephen
I am using an LM2831 to generate 3.3V. The input of the LM2831 is supplied by 5V from the output of another LM2831.