This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
Below is the manual reset introduction. As I know, when Vsense is normal and MR_bar is lower than VMR_bar_low && tMR_bar_w > 1us(datasheet), and then Reset_bar is low. I would like to know, could we adjust the tMR_bar_w from using external circuit? or do we have rest IC which could adjust the tMR_bar_w? (at least 100ms)
By the way, I would like to know, do we have the reset IC which has function of below point
1. for example, Vmon = 1.2 V and has an X pin, if sense volatge = 1V and X pin go high >100ms the reset_bar output=0, if sense volatge = 1V but X pin go high <100ms the reset_bar output=1
Roy,
1: could we adjust the tMR_bar_w from using external circuit?
Answer: tMR_bar_w is caused by the user because /MR is an input. In the above diagram, t_PD(/MR) is fixed, and t_D(/MR) is programmable with capacitor
2:
do we have the reset IC which has function of below point
1. for example, Vmon = 1.2 V and has an X pin, if sense volatge = 1V and X pin go high >100ms the reset_bar output=0, if sense volatge = 1V but X pin go high <100ms the reset_bar output=1
Answer: Yes, we have solution that will work. It uses TPS3895, TPS3896, TPS3897, TPS3898 family. Please email me at michaeldesando@ti.com and I can work with you to provide detailed solution.