This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22916: Input vs output capacitor

Part Number: TPS22916

Dear TI-Team,

We want to use TPS22916 to control a MCU's VUSB input which will only be connect if the board's VIN > 4.5V (VIN could be a USB charger or a solar cell)

in this post
https://e2e.ti.com/support/power-management/f/196/t/740376

 recommends to use an input capacitor with x10 capacitance of the output. Well, the VUSB of the MCU recommends a 10uF cap, but I can't imagine we  had to use a 100uF cap for TPS22916's VIN :)

Please advise

Thanks!

Chris

  • Chris,

    While we recommend a 10:1 input to output capacitor ratio on the device, the reality is that this is based on the power supply’s ability to handle the turn on transients of the device. The TPS22916 has a pretty controlled slew rate. As long as the power supply can handle the turn on of the device, then the 10:1 ratio is not needed (even 1:1 is okay). If the output capacitance is larger than the input capacitance, then if the input drops very suddenly, the output voltage will drop slower than the input and reverse current may flow through the device.

  • Thanks Timothy. I‘ll use 4.7uF out and 10uF in