This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5041: LM5041 Soft start Shut down issue

Part Number: LM5041

HI TI Team,

We are facing soft start shut down issue in LM5041  controller , this project  based on LM5041 current fed push pull converter application circuit. Vin 16 to 40V, Vout :3.3V/50A

At shutdown time COMP goes to down. By the time observed VCC,UVLO,CS pin. All are found normal. Observation: Vin:16V,Vcc above 11V,UVLO above 2.5V, CS pin below 0.5V. 

All reference waveform attached. Kindly share reason for shutdown.Waveform1.xlsx

Regards,

Kubendran