Other Parts Discussed in Thread: UCC28740
I'm trying to design a power supply with the following calculations:
INPUT: 85VAC - 265VAC
OUTPUT: 80 volt, 0.6A
Topology: flyback with opto-coupler feedback
Voltage reference: TL431
controller IC: ucc28740
Transformer (designed using ucc28740 design calculator): PQ26/25 core, Nps = 1.172, Npa = 11.4, Lp = 172.6uH
The datasheet of TL431 states the maximum Vka = 37V, so I assume its not suitable for my use, but I found a flyback power supply design that uses the same TL431 for an output of 110 volts. I'm new to this kind of things hence require help...
thank you!