This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80EVM-020: bq40z80 clear register and data fo a new configuration.

Part Number: BQ40Z80EVM-020
Other Parts Discussed in Thread: BQ40Z80

Hi, I'm using the EVM to understand the functionalities of the BQ40Z80.

I successfully finished a learning cycle for a 2s configuration and a switched to a 3s changing the following parameters:

Number of cells: 3  in Settings, Configuration, Cell configuration
Design Capacity mAh 2950, in Gas Gauging subsection in the Data Memory
Design Capacity cWh  3186, in Gas Gauging subsection in the Data Memory
Design Voltage mV  10800, in Gas Gauging subsection in the Data Memory
Charge Term Taper Current in 150mA ,Advanced Charge Algorithm, Termination Config section of Data Memory
Dsg Current Threshold 100mA in Gas Gauging, Current Thresholds section of Data Memory
Chg Current Threshold 50mA in Gas Gauging, Current Thresholds section of Data Memory
Quit Current 10mA Gas Guaging, in Current Thresholds section of Data Memory
Terminate Voltage mV  7500 mV.  in the Gas Gauging, IT Cfg section of Data Memory

But seems that the BQ40Z80 has the oldest information of the 2s (RSOC 100%, ASOC 0% and other parameters that seems to be incoherents). Voltages and currents are ok. RCA=1.

How can I clean up the configuration? Do I need only antoher learning cycle or should I clean up some register?

Thanks