This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409: Iout couldn't be adjusted based on the surrounding components.

Expert 2415 points
Part Number: LM3409

Hi,

Current facing an issue for LM3409 which based on the specs below and unable to achieve the Iout because the Iout follows the Iin values.When the nput 24Vdc, the output current follow the input current setting on DC power supply. Using Onsemi PFET FQD7P20 in the circuit.

If mean when the input current 2A fromDC power supply, the LED output current also 2A.

Vin: 10 ~ 60VDC > 24Vdc typ.

Vout: 6.6V @ 2.1A

As for schematic and layout is confidential, please provide email in order for me to share the file.

When input 24Vdc, the output current follow the input current setting on DC power supply.
If mean when I set input current 2A on DC power supply, the LED output current also 2A.