Part Number: LP5036
Other Parts Discussed in Thread: LP5030, LP5024
Hello,
I'm working on a medical device that we are trying to expedite into the market for obvious reasons. We're having a problem with multiple boards and I need your help.
The LP5036 is connected to ten (10) RGB LEDs. Each element on the LED gets its own output channel on the LP5036. Yes, we could have used the LP5030 but the LP5036 was more readily available so we are using that for now.
PROBLEM: All red LEDs are on continuously, about 1mA for entire board of 10 red elements. This would be a leakage of about 100uA, far above the specification. This occurs even when the board is totally disconnected from I2C bus; only VLED and VCC are powered.
Riref is set to 10k;
Each LED is Kingbright APFA3010SEEZGKQBKC, forward voltage is 2V Red, 3.3V Green, 3.3V Blue. Physically the Red pin and Common pin are on opposite sides of the package so
VCC is 3.3V. LEDs are powered by 3 'C' batteries, nominal voltage 4.5V.
Supplying both LVCC and LEDs from 3.3V (as a test) results in current draw of 1.07mA. Much higher than leakage current specified.
Tried turning off CHIP_EN in DEVICE_CONFIG0, no change
Tried turnning of LED_GLOBAL_OFF in DEVICE_CONFIG1, no change
Tried toggling hardware EN pin, no change.
Tried halving the value of Riref (to 5k) but no change.
If it was just a random solder problem then I would have expected the other channels (blue & green) to be affected. I also would have expected to see some channels affected but not all.
reGISTERS UPON STARTUP:
LP205xx Register Values:
[0] DEVICE_CONFIG0 = 0x00 [1] DEVICE_CONFIG1 = 0x3C [2] LED_CONFIG0 = 0x00 [3] LED_CONFIG1 = 0x00
[4] BANK_BRIGHT = 0xFF [5] BANK_A_COLOR = 0x00 [6] BANK_B_COLOR = 0x00 [7] BANK_C_COLOR = 0x00
[8] LED0_BRIGHT = 0xFF [9] LED1_BRIGHT = 0xFF [10] LED2_BRIGHT = 0xFF [11] LED3_BRIGHT = 0xFF
[12] LED4_BRIGHT = 0xFF [13] LED5_BRIGHT = 0xFF [14] LED6_BRIGHT = 0xFF [15] LED7_BRIGHT = 0xFF
[16] LED8_BRIGHT = 0xFF [17] LED9_BRIGHT = 0xFF [18] LED10_BRIGHT = 0xFF [19] LED11_BRIGHT = 0xFF
[20] OUT0_COLOR = 0x00 [21] OUT1_COLOR = 0x00 [22] OUT2_COLOR = 0x00 [23] OUT3_COLOR = 0x00
[24] OUT4_COLOR = 0x00 [25] OUT5_COLOR = 0x00 [26] OUT6_COLOR = 0x00 [27] OUT7_COLOR = 0x00
[28] OUT8_COLOR = 0x00 [29] OUT9_COLOR = 0x00 [30] OUT10_COLOR = 0x00 [31] OUT11_COLOR = 0x00
[32] OUT12_COLOR = 0x00 [33] OUT13_COLOR = 0x00 [34] OUT14_COLOR = 0x00 [35] OUT15_COLOR = 0x00
[36] OUT16_COLOR = 0x00 [37] OUT17_COLOR = 0x00 [38] OUT18_COLOR = 0x00 [39] OUT19_COLOR = 0x00
[40] OUT20_COLOR = 0x00 [41] OUT21_COLOR = 0x00 [42] OUT22_COLOR = 0x00 [43] OUT23_COLOR = 0x00
[44] OUT24_COLOR = 0x00 [45] OUT25_COLOR = 0x00 [46] OUT26_COLOR = 0x00 [47] OUT27_COLOR = 0x00
[48] OUT28_COLOR = 0x00 [49] OUT29_COLOR = 0x00 [50] OUT30_COLOR = 0x00 [51] OUT31_COLOR = 0x00
[52] OUT32_COLOR = 0x00 [53] OUT33_COLOR = 0x00 [54] OUT34_COLOR = 0x00 [55] OUT35_COLOR = 0x00
AFTER TURNING OFF LED GLOBAL OFF:
issue persists:
LP205xx Register Values:
[0] DEVICE_CONFIG0 = 0x40 [1] DEVICE_CONFIG1 = 0x01 [2] LED_CONFIG0 = 0x00 [3] LED_CONFIG1 = 0x00
[4] BANK_BRIGHT = 0xFF [5] BANK_A_COLOR = 0x00 [6] BANK_B_COLOR = 0x00 [7] BANK_C_COLOR = 0x00
[8] LED0_BRIGHT = 0xFF [9] LED1_BRIGHT = 0xFF [10] LED2_BRIGHT = 0xFF [11] LED3_BRIGHT = 0xFF
[12] LED4_BRIGHT = 0xFF [13] LED5_BRIGHT = 0xFF [14] LED6_BRIGHT = 0xFF [15] LED7_BRIGHT = 0xFF
[16] LED8_BRIGHT = 0xFF [17] LED9_BRIGHT = 0xFF [18] LED10_BRIGHT = 0xFF [19] LED11_BRIGHT = 0xFF
[20] OUT0_COLOR = 0x00 [21] OUT1_COLOR = 0x1F [22] OUT2_COLOR = 0x00 [23] OUT3_COLOR = 0x00
[24] OUT4_COLOR = 0x1F [25] OUT5_COLOR = 0x00 [26] OUT6_COLOR = 0x00 [27] OUT7_COLOR = 0x1F
[28] OUT8_COLOR = 0x00 [29] OUT9_COLOR = 0x00 [30] OUT10_COLOR = 0x1F [31] OUT11_COLOR = 0x00
[32] OUT12_COLOR = 0x00 [33] OUT13_COLOR = 0x1F [34] OUT14_COLOR = 0x00 [35] OUT15_COLOR = 0x00
[36] OUT16_COLOR = 0x1F [37] OUT17_COLOR = 0x00 [38] OUT18_COLOR = 0x00 [39] OUT19_COLOR = 0x1F
[40] OUT20_COLOR = 0x00 [41] OUT21_COLOR = 0x00 [42] OUT22_COLOR = 0x1F [43] OUT23_COLOR = 0x00
[44] OUT24_COLOR = 0x00 [45] OUT25_COLOR = 0x1F [46] OUT26_COLOR = 0x00 [47] OUT27_COLOR = 0x00
[48] OUT28_COLOR = 0x1F [49] OUT29_COLOR = 0x00 [50] OUT30_COLOR = 0x00 [51] OUT31_COLOR = 0x00
[52] OUT32_COLOR = 0x00 [53] OUT33_COLOR = 0x00 [54] OUT34_COLOR = 0x00 [55] OUT35_COLOR = 0x00
[56] RESET = 0x00....(tick)#........(tick)#.