Hi team,
My customer has been using TPS54335A and provided some questions as follows.
- The datasheet says that minimum off time is 0% under condition that Vboot-ph>3V in section 6.7.
Does this mean the device can work at 100% duty cycle as long as Vboot-ph keeps above 3V? - The datasheet says that "When the voltage between BOOT and PH pins drops below the BOOT-PH UVLO threshold, which is 2.1 V (typical), the high-side MOSFET turns off and the low-side MOSFET turns on, allowing the boot capacitor to recharge" in section 7.3.9.
How long time does it take for recharge when Vboot-ph drops below BOOT-PH UVLO threshold? - Refering to equation (2), when the customer set Vstart is lower than target output voltage, does device work correctly?
e.g. Vstart=7.5V, target Vout=9V - Under condition that target output voltage is higher than input voltage, does device work correctly at 100% duty cycle?
(Except for recharge time for bootstrap capacitor.)
I'm looking forward to hearing back from you.
Best regards,
Shota Mago