This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM33606: Complression limits for LMZM33606 under an heat sink

Part Number: LMZM33606

Dear all,

I need to use a thermal pad on the top of a LMZM33606 in order connect it to a heat sink and remove as much heat as possible. 

Can you tell me what's the compression resistance of this device once mounted on a PCB?

Because I cannot use thermal paste and thermal pads require mounting pressures between 10 and 40 PSI in order to reach good performances. This means that I will compress the power module with a total force between 12 N and 45 N. Im not aware of the common mechanical resistance of such a device.

Thanks and kind regards,

Efraim Brandolini