Other Parts Discussed in Thread: TPS2493, TPS25982, LM5060, LM5069, INA282, TPS1663
I am evaluating the TSP2493 using the EVM-002 board.
We plan to use the part with an MCU and monitor the output current, and use the UVEN line to control the output.
During my testing, using the ENA/DIS switch on the PCB, I noted that sometimes the IMON output would go to full scale for about 200uS immediately after being enabled. To speed testing and eliminate any variables due to manual switching, I connected a signal generator to the UVEN line (see attached PDF). For this testing, no load was attached to the PCB. The only circuit elements present on VOUT are C3, C9 and D2 as indicated in the EVM schematic.
What I then observed, is that depending on the PRF (repetition frequency), IMON either glitches, or does not glitch, immediately after UVEN goes high. For example, at 5.0Hz PRF, IMON behaves correctly when UVEN is asserted. At 5.1Hz, IMON goes full-scale for 200uS every time UVEN is asserted. I observed this behavior from as low as 0.7Hz, to as high as 20Hz, with variations in PRF from 0.01 to 0.1Hz causing a change in IMON behavior. There are 3 scope plots in the attached PDF. The two plots that show IMON indicate a small damped hump starting about 400uS after UVEN is asserted. This is the charging current of the capacitor(s) on VOUT. The third plot shows that VOUT has not begun to turn on yet when IMON goes full scale. All other signals (FAULT, PG, TIMER), maintain a steady value throughout the ON period. In other words, no other operation anomalies are observed, it seems that the IMON output is the only affected signal.
Thanks for any insights,
Will