Hi all.
I have to design an isolated power stage with these requirements:
- Vin: nominal 12V, min/max: 10/15V
- Vout: 24V nominal (not a strict requirement: any voltage between 20 and 28 V is ok for me)
- Iout: 40-50 mA typical, 110 mA maximum
- 1 kV functional isolation (2.5 kV would be better)
- the temperature could go up to 60 °C
- maximum possible efficiency
I used Webench in order to find a possible device and I found a design based on LM25180, with a 91% efficiency rating (very good for me). But I have to use an off-the-shelf transformer, and the ones suggested are far too big. I found some devices: Wurth Elektronik 7448845470, Bourns SRF1260-220M, etc (many have different devices in the same series, so there are many possible choices). Are they ok? What should I look for in order to find a suitable alternative transformer?
Thanks in advance.
Best regards,
Stefano Infante